Setting the network or MAC address - Triatek - LIT-12014409 - HMS1655 Fume Hood Controller

HMS1655 Fume Hood Controller User Guide

Product
Controls > Fume Hood Controls > HMS1655 Fume Hood Controller
Document number
LIT-12014409
Revision date
2024-05-27
Product status
Discontinued

The Set Address option on the Network Setup menu enables specification of the network or MAC address as required. For BACnet MS/TP networks, the valid range of MAC addresses that support master node is 1 to127. For Metasys N2 Open networks, the valid range of network addresses is 1 to 255.

The Set Address option on the Network Setup menu opens the Enter MAC Address configuration screen if the unit is configured for BACnet protocol support. Otherwise, the Enter Network Address configuration screen appears and prompts the user for a new Metasys N2 subordinate address.