Setting the baud rate - Triatek - LIT-12014409 - HMS1655 Fume Hood Controller

HMS1655 Fume Hood Controller User Guide

Product
Controls > Fume Hood Controls > HMS1655 Fume Hood Controller
Document type
User Guide
Document number
LIT-12014409
Revision date
2024-05-27
Product status
Discontinued

You can use the Set Baud Rate option on the Network Setup menu to enable baud rate configuration by the connected HMS1655 network. This menu option is only available if the unit is configured for BACnet protocol support. The Set Baud Rate option opens the Select Baud Rate configuration screen.