Configuring network settings - Triatek - LIT-12014409 - HMS1655 Fume Hood Controller

HMS1655 Fume Hood Controller User Guide

Product
Controls > Fume Hood Controls > HMS1655 Fume Hood Controller
Document number
LIT-12014409
Revision date
2024-05-27
Product status
Discontinued
The Network Setup menu enables configuration of settings associated with the network capabilities of the HMS1655. This includes:
  • Network or MAC address selection
  • Baud rate parameters specification
  • BACnet protocol specification
  • Configuration of any protocol-specific settings
You can select one of four standard baud rates and set the MAC address for the HMS1655.