Configuring hood settings - Triatek - LIT-12014409 - HMS1655 Fume Hood Controller

HMS1655 Fume Hood Controller User Guide

Product
Controls > Fume Hood Controls > HMS1655 Fume Hood Controller
Document number
LIT-12014409
Revision date
2024-05-27
Product status
Discontinued

The Fume Hood Setup menu, as shown in naf1709553836979.html#naf1709553836979__fig_zxd_knn_q1c, supports the configured fume hood settings. This includes field calibration of the face velocity sensor, selection of the hood operating mode, configuration of the setpoints for occupied, unoccupied, and decommissioned modes of operation, and the ExAccel capability set up.

The Field Calibration option supports calibration for the sidewall sensor that measures the face velocity at the sash opening of the fume hood. You can use the operating mode of the monitored fume hood to toggle between occupied, unoccupied, and decommissioned modes. The Edit Setpoints option supports target setpoints configuration for all three operating modes of the fume hood. The ExAccel Setup option enables configuration of ExAccel mode, which accelerates the speed at which the control output adjusts to compensate for the opening or closing sash.

Figure 1. Fume hood setup