Configuring controller settings - Triatek - LIT-12014409 - HMS1655 Fume Hood Controller

HMS1655 Fume Hood Controller User Guide

Product
Controls > Fume Hood Controls > HMS1655 Fume Hood Controller
Document number
LIT-12014409
Revision date
2024-05-27
Product status
Discontinued

The Controller Setup menus provide access to facilities for configuration all of the settings associated with the HMS1655 when set up as a fume hood controller. The menu also includes analog input and output set up, alarm relay set up, PID loop settings configuration, alarm setpoints, audible alert settings, and engineer units for the face velocity reading selection.