About this task
Figure 1. Single Sensor Mode
Procedure
- To change the name of the monitored fume hood, tap the screen anywhere on the current name. You can use the alphanumeric popup keyboard that appears to modify the name. After you edit the fume hood name, tap Save.
- To change the current operating mode of the monitored fume hood, tap the screen at the current hood status line. The Set Operating Mode configuration screen appears.
- If you store at least one security password in the system, tap the current operating mode to open the password entry popup before you change the mode of operation. This prevents inadvertent change to the operating mode by unauthorized personnel.
- To change the current displayed units for the fume hood face velocity reading, tap on the existing units ft/min or m/sec to provide access to the Engineering Units menu option on the Controller Settings menus.
- To set the time and date displayed at the bottom of the main screen, tap them individually and enter the new settings.