Setting the backlight intensity - Triatek - LIT-12014409 - HMS1655 Fume Hood Controller

HMS1655 Fume Hood Controller User Guide

Product
Controls > Fume Hood Controls > HMS1655 Fume Hood Controller
Document type
User Guide
Document number
LIT-12014409
Revision date
2024-05-27
Product status
Discontinued

Procedure

  1. Tap the Set Brightness option on the Display Setup menus to open the Set Backlight Level popup slider.
  2. To increase the brightness of the display, move the slider to the left. To decrease the brightness, move the slider to the right.
  3. Tap OK to save the new brightness setting to non-volatile memory in the event of power loss.