Selecting the display options - Triatek - LIT-12014409 - HMS1655 Fume Hood Controller

HMS1655 Fume Hood Controller User Guide

Product
Controls > Fume Hood Controls > HMS1655 Fume Hood Controller
Document type
User Guide
Document number
LIT-12014409
Revision date
2024-05-27
Product status
Discontinued

About this task

You can use the Display Options to customize the main display of the HMS1655 and select the sources for each of the displayed parameters. This option opens the Set Display Options configuration popup.

Procedure

  1. If the HMS1655 does not monitor temperature, clear Temperature on the Set Display Options configuration popup.
  2. If the sash position is not monitored, deselect the Sash Position. The other parameters are always available, but you can disable them from the display.
  3. When you select the displayed parameters, tap Next to open the Select Source for Temperature Display configuration popup to specify the source input for the temperature display.
    Note: The default source for the temperature display is Thermistor Input 1.
  4. To retrieve the temperature from the network and display on the main screen, tap Network Variable on the configuration popup.