Modifying input names - Triatek - LIT-12014409 - HMS1655 Fume Hood Controller

HMS1655 Fume Hood Controller User Guide

Product
Controls > Fume Hood Controls > HMS1655 Fume Hood Controller
Document number
LIT-12014409
Revision date
2024-05-27
Product status
Discontinued

About this task

You can label the HMS1655 analog and thermistor inputs with custom names to more accurately describe the location or type of each input.

Procedure

  1. To edit each of the default names associated with the analog and thermistor inputs, tap Display Setup > Edit Input Names > Input Names Setup
  2. On the Input Names Setup menu, choose one of the analog inputs or thermistor inputs to open the alphanumeric popup keyboard.
  3. Use the keyboard to edit the current name and customize the specific application of that particular input on the HMS1655.
  4. Tap the orange button between the Cancel and Save buttons to toggle between uppercase, lowercase, and numeric characters.