Using the Real-Time View option - Triatek - LIT-12014409 - HMS1655 Fume Hood Controller

HMS1655 Fume Hood Controller User Guide

Product
Controls > Fume Hood Controls > HMS1655 Fume Hood Controller
Document number
LIT-12014409
Revision date
2024-05-27
Product status
Discontinued

About this task

The HMS1655 incorporates a feature for the installer or commissioning technician to view the real-time conditions of all of the hardware resources and several system variables. This includes the universal analog inputs, dedicated thermistor inputs, universal analog outputs, digital inputs, relay outputs, alarm status for each analog and thermistor input, and the four network variables for pressure, temperature, humidity, and air changes.

Procedure

  1. To view the real-time conditions of any of the listed resources, tap Diagnostics > Real-Time View .
  2. To open the real-time view configuration screen, tap Real-Time View > Analog Inputs.
  3. To skip to the next set of resources to view, tap Next.
  4. To cancel the real-time view display at any time, tap Exit to return to the Real-Time View menu.
    Note: You can use the Alarm Status option on the second page of the Real-Time View menu to monitor the alarm status for each universal analog input and the two thermistor inputs in real-time. You can monitor the real-time conditions of the four network variables for face velocity, temperature, humidity, and air changes with the Network Vars option on the second page of the Real-Time View menus.