Retrieving system information - Triatek - LIT-12014409 - HMS1655 Fume Hood Controller

HMS1655 Fume Hood Controller User Guide

Product
Controls > Fume Hood Controls > HMS1655 Fume Hood Controller
Document number
LIT-12014409
Revision date
2024-05-27
Product status
Discontinued

The About This HMS option on the Diagnostics menus provides information specific to the specific unit, including firmware version numbers, electronic serial numbers, protocol selection, and network address. For more information, see Retrieving system information.

Figure 1. About pop up screen