Figure 1. DIP switch settings
Figure 2. DIP switch functions
Note: DIP Switch function, other than address and
termination, can be disabled by internal software setting and selection.
Switch | On | Off | If enabled |
---|---|---|---|
1 | +1 | 0 | Unit hardware address 0-15 |
2 | +2 | 0 | Unit hardware address 0-15 |
3 | +4 | 0 | Unit hardware address 0-15 |
4 | +8 | 0 | Unit hardware address 0-15 |
5 | Reverse | Normal | Actuator reverse/normal |
6 | CFM | Position | Input = position/CFM |
7 | CFM | Position | Output = position/CFM |
8 | Terminate | Open | RS485 line terminate |