Controller state settings - Titus - LIT-12014051 - Valve - Venturi Valve

Titus Venturi Air Valve Installation Guide

Brand
Titus
Product name
Venturi Valve
Document type
Installation Guide
Document number
LIT-12014051
Revision date
2023-04-05
Language
English

The User Settings tab selects the various operational states of the UVM. The tab states are permanent, non-permanent, and status.

Table 1. User state settings
Operational states Description
Permanent state Can be set or unset in the UVM. The permanent state settings are stored in EEPROM. The settings retain their state across power losses.
Non-permanent state Can be set from the tool but resets to unselected when the power to UVM is cycled. They are typically used for overrides and tests.
Status Advisory states used for debugging.