Status - Titus - LIT-12014051 - Valve - Venturi Valve

Titus Venturi Air Valve Installation Guide

Brand
Titus
Product name
Venturi Valve
Document type
Installation Guide
Document number
LIT-12014051
Revision date
2023-04-05
Language
English

The DI State setting indicates status only. If the user clicks the check box it has no effect on the UVM. When you click the Get All State Settings button, the configuration tool reads through all the states that are set and not set in the UVM. The state of the UVM DI_1 input reflects the final state of the check box.

The Digital Sensor OK setting indicates the status of the digital sensor when the digital sensor is enabled with the Use Digital Sensor setting in the Permanents group. If the user clicks the Get All State Settings button, the configuration tool reads through all the states that are set and not set in the UVM. The State of the Digital Sensor operation reflects the final state of the check box.