Raw AI values - Titus - LIT-12014051 - Valve - Venturi Valve

Titus Venturi Air Valve Installation Guide

Brand
Titus
Product name
Venturi Valve
Document type
Installation Guide
Document number
LIT-12014051
Revision date
2023-04-05
Language
English

The raw AI 1 (SP) fields display the raw value on the IN setpoint analog input. The first field is the actual A/D count from the IN analog input. The second field is the input value as a percentage of the total possible input range.

The input value is between 0 and 4095. The second field is the input A/D as a percentage of 4095. The third field is 4095 of A/D input as a percentage of 4095. You can use the values as a rough guide to where the input signal is relative to the full range.

The raw AI 0 (Fb) fields display the raw value on the feedback sensor analog input. The first field is the actual A/D count from the feedback analog input. The second field is the input value as a percentage of the total possible input range. The input value is between 0 and 4095. The second field is the input A/D as a percentage of 4095.

The third field is 4095 of A/D input as a percentage of 4095. You can use the values as a rough guide as to where the feedback signal is relative to the full range.

In normal operation, the IN signal goes from 0 V to 10 V, or 0 to 4095. If you position the actuator differently and it has a different angular range on the valve, the feedback signal may use only a portion of the range.

The raw AI 2 (Press) fields display the raw value on the analog sensor pressure analog input.

The first field is the actual A/D count from the press sensor analog input. The second field is the input value as a percentage of the total possible input range.