Dynamic values tab - Titus - LIT-12014051 - Valve - Venturi Valve

Titus Venturi Air Valve Installation Guide

Brand
Titus
Product name
Venturi Valve
Document type
Installation Guide
Document number
LIT-12014051
Revision date
2023-04-05
Language
English

The dynamic values tab provides a set of buttons and fields to access dynamic values within the controller.

The tab finds faults and debugs performance issues. Output override values can also be set from here. If selected, you can enter a soft setpoint.

The values displayed include calculated values such as CFM, position, and pressure. Also displayed are raw A/D values from the AI inputs. The values do not automatically update. To read a value, click the associated value button.