User settings tab - Titus - LIT-12014051 - Valve - Venturi Valve

Titus Venturi Air Valve Installation Guide

Brand
Titus
Product name
Venturi Valve
Document type
Installation Guide
Document number
LIT-12014051
Revision date
2023-04-05
Language
English

The User Settings tab enables the user to configure settings for the UVM. The tab's settings depend on which mode of operation is required and what options can be enabled.

For specific information to be loaded to the controller, use the individual Set buttons.

Note: Do not overwrite factory calibration values in the UVM for the AO and AI ports.