Misc tab - Titus - LIT-12014051 - Valve - Venturi Valve

Titus Venturi Air Valve Installation Guide

Brand
Titus
Product name
Venturi Valve
Document type
Installation Guide
Document number
LIT-12014051
Revision date
2023-04-05
Language
English

The Misc tab enables the user to read and write all the settings from the UVM.

The serial number, module revision, and calibration date can be viewed on the Misc tab.

To change the serial number and calibration date on the unit, click Set Serial Number or Set Calibration Date buttons. For a visual example, see Figure 33.

You can set the alternate address of the module as well. The unit responds to both the DIP switch set address and the software set alternate address. The DIP address can be used for initial setup and small clusters of UVMs. If more than 16 units are on the bus, use the software alternate address.

Note: When using Write ALL Settings to Device on a new device, do not overwrite the existing calibration information.
  1. Set the address of the UVM module you want to interact with from addresses 0 to 15. The addresses are from the DIP switches on the unit. See the UVM Installation Guide for more information.
    Note: The unit can have an internal soft address, labeled 6 to 255, that it responds to automatically.
  2. To confirm that communication is present, click Get Revision. The revision number appears in the Misc tab module revision box.
  3. To save a copy of these settings to your computer, click Save Displayed Values to File.
    Note: The Save Displayed Values to File button saves the configuration software values. The button does not save values in the UVM. To save the values in the UVM, click the Get All Settings From Device button when you have received the setting.