Module calibration information - Titus - LIT-12014051 - Valve - Venturi Valve

Titus Venturi Air Valve Installation Guide

Brand
Titus
Product name
Venturi Valve
Document type
Installation Guide
Document number
LIT-12014051
Revision date
2023-04-05
Language
English
The factory uses module calibration information for setup of the UVM. The field enables the importation of the valve curves and valve data for inclusion in the UVM storage. The field also creates valve summary labels. You can calibrate the feedback sensor from the CFM Table tab.
Note: Do not use this field unless under instruction from Triatek.