Introduction - Titus - LIT-12014051 - Valve - Venturi Valve

Titus Venturi Air Valve Installation Guide

Brand
Titus
Product name
Venturi Valve
Document type
Installation Guide
Document number
LIT-12014051
Revision date
2023-04-05
Language
English

The Titus Universal Valve Module is designed to enable interoperability between Titus Venturi valves and third party controllers.

Each Titus valve is individually calibrated and has its own unique position to cubic feet per minute (CFM) curve. The UVM enables you to create a linearization curve in each controller for each associated valve. It also enables you to span, scale, and linearize the feedback sensor to obtain useful information from the UVM.