DP switch connections - Titus - LIT-12014051 - Valve - Venturi Valve

Titus Venturi Air Valve Installation Guide

Brand
Titus
Product name
Venturi Valve
Document type
Installation Guide
Document number
LIT-12014051
Revision date
2023-04-05
Language
English

A pressure sensor is used to determine the pressure across the valve and reduce the CFM feedback signal to zero when the pressure falls below a preset threshold. The UVM Configuration Tool scales the pressure sensor input, enables the pressure sensor, and defines the lower pressure threshold. The pressure sensor wiring is shown in the Figure 29 below. .

Figure 1. Pressure sensor wiring