Installation and setup - Titus - LIT-12014051 - Valve - Venturi Valve

Titus Venturi Air Valve Installation Guide

Brand
Titus
Product name
Venturi Valve
Document type
Installation Guide
Document number
LIT-12014051
Revision date
2023-04-05
Language
English

The 24 VAC supply needs to provide a minimum of 25 VA, with 20 VA for the actuator and 5 VA for the UVM. The 0 V to 10 V CFM request signal is attached to the IN connection on the UVM board, with the ground lead going to any of the GND connections. The feedback signal is derived from the Vo connection and any of the GND connections. For more information on wiring requirements, see Figure 16.