Mounting the flanged valve - Titus - LIT-12014051 - Valve - Venturi Valve

Titus Venturi Air Valve Installation Guide

Product
Valves and Actuators > Valves > Venturi Valve
Document type
Installation Guide
Document number
LIT-12014051
Revision date
2023-04-05

Flanged valves require a gasket between the duct and valve flanges, with the addition of nuts and bolts as flange fasteners. Ensure that the metal straps support both sides of the valve weight and the duct work. For correct hardware, mounting, sealing and installation requirements, consult local building codes.

Note: Gasket, nuts, and bolts are field supplied. They do not come with the valve.
Figure 1. Mounting a flanged valve