Dimensions - PENN Controls - LIT-12013344 - TC3221 - TC3222 - TC3223 - TC3224N9R - TC3B21 - TC3B22 - TC3B23 - TC3X21 - Electronic Refrigeration, Defrost, and Multi-Purpose Controller - TC Series Panel-Mount Refrigeration Controller

Penn TC Series Refrigeration and Defrost Controller Product Bulletin

brand
PENN Controls
prodname
TC Series Panel-Mount Refrigeration Controller
doctype
Product Bulletin
docnumber
LIT-12013344
revised_modified
2020-09-01

The following figures show the TC controller dimensions and the panel cut-out dimensions that you require to insert the TC controller into the panel.

Figure 1. TC3B and TC3 controller dimensions, mm (in.)

Figure 2. TC3X controller dimensions, mm (in.)