Applications - PENN Controls - LIT-12013344 - TC3221 - TC3222 - TC3223 - TC3224N9R - TC3B21 - TC3B22 - TC3B23 - TC3X21 - Electronic Refrigeration, Defrost, and Multi-Purpose Controller - TC Series Panel-Mount Refrigeration Controller

Penn TC Series Refrigeration and Defrost Controller Product Bulletin

brand
PENN Controls
prodname
TC Series Panel-Mount Refrigeration Controller
doctype
Product Bulletin
docnumber
LIT-12013344
revised_modified
2020-09-01

You can use the TC controller for the following applications:

Table 1. TC controller applications
Model number Application
TC3X21N5V Upright commercial refrigerators, food prep-tables, under-counter refrigerators
TC3B21N5V Upright commercial refrigerators, food prep-tables, under-counter refrigerators
TC3B22N5V Commercial refrigerators, back-bar units, glass-door display cases
TC3B23N5V Upright commercial freezers, ice cream freezers, bottle coolers
TC3B54N9V Upright commercial freezers, ice cream freezers, or bottle coolers with variable speed compressors
TC3221N5V Upright commercial refrigerators, food prep-tables, under-counter refrigerators
TC3222N5V Commercial refrigerators, saladettes, back-bar units, glass-door display cases
TC3223N5V Upright commercial freezers, ice cream freezers, bottle coolers, c-store coolers and freezers
TC3224N9R Glass-door upright freezers, refrigerated display cases, walk-in coolers and freezers, c-store coolers and freezers

Important: Use the TC Series controller only as an operating control. Where failure or malfunction of the TC controller could lead to personal injury or property damage to the controlled equipment or other property, additional precautions must be designed into the control system. Incorporate and maintain other devices, such as supervisory or alarm systems or safety or limit controls, intended to warn of or protect against failure or malfunction of the TC controller.
Important : Utiliser ce TC Series Controller uniquement en tant que dispositif de contrôle de fonctionnement. Lorsqu'une défaillance ou un dysfonctionnement du TC Controller Régulateur risque de provoquer des blessures ou d'endommager l'équipement contrôlé ou un autre équipement, la conception du système de contrôle doit intégrer des dispositifs de protection supplémentaires. Veiller dans ce cas à intégrer de façon permanente d'autres dispositifs, tels que des systèmes de supervision ou d'alarme, ou des dispositifs de sécurité ou de limitation, ayant une fonction d'avertissement ou de protection en cas de défaillance ou de dysfonctionnement du TC Régulateur.