Parts included - Romutec - LIT-12014235 - JDB8410-1 - Manual and Installation Instructions - JDB8410-1 Input/Output Module - 4.04

JDB8410-1 Input/Output Module Installation Guide

Product
Document type
Installation Guide
Document number
LIT-12014235
Version
4.04
Revision date
2023-04-26
Product status
Active
  • One JDB8410-1 Input/Output Module with removable terminal plug
  • One installation guide
  • Optional: one JDB8420 front panel module, if ordered
  • Optional: one rail-mounted JDB8440 module, if ordered
  • Optional: one USB cable type A-B, only delivered with JDB8420 or JDB8440