Observe the following guidelines to mount
the JDB8410-1, JDB8420, and JDB8440 modules:
- Mount the modules in areas free of corrosive vapors and observe the environmental limitations listed in the Technical specifications section.
- Do not mount the modules on surfaces that are prone to vibration.
- Do not mount the modules in areas where electromagnetic emissions from other devices or wiring can interfere with the modules' communication.
- Mount the modules so that no other parts or devices obstruct ventilation or radiate heat into the modules' housing.