Installation - Romutec - LIT-12014235 - JDB8410-1 - Manual and Installation Instructions - Romutec - 4.04

JDB8410-1 Input/Output Module Installation Guide

Brand
Romutec
Product name
Romutec
Document type
Installation Guide
Document number
LIT-12014235
Version
4.04
Revision date
2023-04-26
Product status
Active
Language
English
Observe the following guidelines when you install the JDB8410-1, JDB8420, and JDB8440 modules:
  • Transport the modules in the original container to minimize vibration and shock damage to the devices.
  • Do not drop the JDB device or expose it to physical shock.
  • Verify that the modules include all parts listed in the following section.