Display Code - PENN Controls - VFD68Bxx - VFD68Cxx - VFD68Dxx - Three‐Phase Motor Speed Controller - VFD68 Three‐Phase Variable Frequency Drive

VFD68 Variable Frequency Drives Technical Bulletin

Product
Document revision
C
Revision date
2019-08-09
Part number
24-7664-3051

Parameter Setting Mode: When the display shows Pr.., the VFD68 drive displays parameter codes and parameter setting values.

  • Press Up or Down to scroll through the parameter codes and to edit parameter setting values.
  • Press SET to enter the 3-digit parameter code for viewing and editing.
    Figure 1. Operation Panel

    Table 1. Operation Panel Keys
    Key Description
    RUN Used to give a start rotation command.
    STOP/RESET
    • Used to stop operation.

    • Used to reset the VFD68 Drive when the output stops due to activation of the protection function.

    MODE Used to select the operation mode or setting mode.
    SET Used to determine the frequency and parameter settings.
    Up/Down
    • Used to increase or decrease the running frequency consecutively. Hold down the key to change the frequency.

    • Used to change the parameter setting consecutively, when in the setting mode. Press the key to change the parameter setting.

    FWD Used to give a forward rotation command.
    REV Used to give a reverse rotation command.
    STOP/RESET
    • Used to stop operation.

    • Used to reset the VFD68 Drive when the output stops due to activation of the protection function.

    Table 2. Unit Indications and Operating Status Indications
    Indication Description
    Hz Lit to indicate frequency
    A Lit to indicate the current (Amperes)
    RUN Lit to indicate drive operation

    Steady light = forward rotation

    Flickering light = reverse rotation

    MON Lit to indicate monitor display mode
    PU Lit to indicate the PU operation mode
    EXT Lit to indicate the external operation mode