The RUN, MON, and PRM LEDs provide drive status and indicate the type of information being displayed on the operation panel monitor.
RUN LED: The LED state (on steady, flashing, or flickering) provides information regarding the drive and motor run status. See Figure 1 for more information.
MON LED: Indicates that the monitor is displaying the drive’s run status. Press (SET) to scroll through run frequency, output amperes, and output voltage.
PRM LED: Indicates that the monitor is set to display parameters and parameter values and allows you to view and edit parameter values.
Figure 1. Operation Panel