Select and Change Most Parameters - PENN Controls - VFD68Bxx - VFD68Cxx - VFD68Dxx - Three‐Phase Motor Speed Controller - VFD68 Three‐Phase Variable Frequency Drive
VFD68 Variable Frequency Drives Technical Bulletin
- Product
- Document revision
- C
- Revision date
- 2019-08-09
- Part number
- 24-7664-3051
Procedure
-
Press MODE until Pr.. PU appears.
-
To change Parameter 32, press UP multiple times until
P.032 appears.
-
Press SET to show 12.5 (default
value of P. 32).
-
Press and hold Down until 9999 appears (9999 indicates
that the motor is set to run at minimum speed and not turn off during a low
pressure condition).
-
Press SET and hold for two seconds to set the new
value.
-
Press SET again to advance to the next parameter.
-
To change additional parameters, press Up or
Down.