Exit the Parameter Adjustment Mode - PENN Controls - VFD68Bxx - VFD68Cxx - VFD68Dxx - Three‐Phase Motor Speed Controller - VFD68 Three‐Phase Variable Frequency Drive

VFD68 Variable Frequency Drives Technical Bulletin

Product
Document revision
C
Revision date
2019-08-09
Part number
24-7664-3051

Procedure

  1. When done, cycle power or press MODE until PU PU appears on the display, then press UP until OP.nd EXT appears on the display.
  2. Press MODE until 0.00 MON EXT appears on the display.
  3. Use the jumper wire to connect terminal SD to terminal STF to run the motor using analog inputs.