Enter the Parameter Adjustment Mode - PENN Controls - VFD68Bxx - VFD68Cxx - VFD68Dxx - Three‐Phase Motor Speed Controller - VFD68 Three‐Phase Variable Frequency Drive

VFD68 Variable Frequency Drives Technical Bulletin

Product
Document type
Technical Bulletin
Document revision
C
Revision date
2019-08-09
Part number
24-7664-3051

Procedure

  1. Remove the jumper that connects terminal SD to terminal STF.
    Important: Remove the jumper to stop the motor before you change the parameter values.
  2. Turn the power on. The monitor display appears.
  3. Open the operation panel cover to reveal more keys.
  4. Press MODE until OP.nd EXT appears on the display, then press UP until PU PU appears.