Procedure
-
Turn
to select a parameter number on the display. Example: P. 32
- Press SET to show the parameter value. (The default value for P. 32 is 12.5.)
-
Turn
to change the parameter value. (Set P. 32 to 9999 if the motor is to run at minimum speed during low pressure events.)
- Press SET twice to store the new value.
-
Press SET again to show the next parameter.
To select and change the value of another parameter, repeat Step 1 through Step 5.
To adjust the C-Prefix parameters, go to Step 1 of Select and Change C-Prefix Parameters. If finished, go to Step 1 of Exit the Parameter Adjustment Mode.