Select and Change C-Prefix Parameters - PENN Controls - VFD68Bxx - VFD68Cxx - VFD68Dxx - Three‐Phase Motor Speed Controller - VFD68 Three‐Phase Variable Frequency Drive

VFD68 Variable Frequency Drives Technical Bulletin

Product
Document revision
C
Revision date
2019-08-09
Part number
24-7664-3051

Procedure

  1. Turn until C... appears.
  2. Press SET. C--- appears.
  3. Turn slightly until the C-prefix parameter that you want to change appears. See Table 1.
  4. Press SET, then turn slightly to read the present set value.
  5. Turn again to change the parameter value.
  6. Press SET twice to store the new value. C--- appears on the LED display.

    To select and change the value of another C-prefix parameter, repeat Step 3 through Step 6.