Exit the Parameter Adjustment Mode - PENN Controls - VFD68Bxx - VFD68Cxx - VFD68Dxx - Three‐Phase Motor Speed Controller - VFD68 Three‐Phase Variable Frequency Drive

VFD68 Variable Frequency Drives Technical Bulletin

Product name
VFD68 Three‐Phase Variable Frequency Drive
Document type
Technical Bulletin
Document revision
C
Revision date
2019-08-09
Part number
24-7664-3051

Procedure

  1. Press MODE twice to exit parameter setting mode (PRM mode) and enter manual operation mode (PU mode). The PU LED illuminates.
  2. Press PU/EXT twice to exit PU mode and enter EXT RUN mode for normal operation. The EXT LED illuminates.
  3. Use the jumper wire to connect terminal SD to terminal STF to run the motor using the analog input.