Enter the Parameter Adjustment Mode - PENN Controls - VFD68Bxx - VFD68Cxx - VFD68Dxx - Three‐Phase Motor Speed Controller - VFD68 Three‐Phase Variable Frequency Drive

VFD68 Variable Frequency Drives Technical Bulletin

Product
Document revision
C
Revision date
2019-08-09
Part number
24-7664-3051

Procedure

  1. Remove the jumper that connects terminal SD to terminal STF.
    Important: Remove the jumper to stop the motor before you change the parameter values.
  2. Turn the power on. The monitor display appears. (The VFD68 drive is in EXT Mode.)
  3. Press PU/EXT to exit EXT mode and go to PU mode (manual override operation mode). The PU LED illuminates.
  4. Press MODE to select PRM mode (parameter setting mode). The PRM LED illuminates.
    Note: See Table 1 for information on the parameters.