WARNING
Avertissement
CAUTION
ATTENTION
Observe the following location guidelines:
- Ensure that the mounting surface can support the VFD, mounting hardware, and any user-supplied panel or enclosure.
- Mount the VFD on flat, even surfaces.
- Allow sufficient space for wires and connections.
- Do not mount the VFD on surfaces that are prone to vibration or in locations where radio frequency or electromagnetic emissions may cause interference.
- Do not install the VFD in an airtight enclosure.
- Do not install heat-generating devices that may cause the temperature to exceed the ambient operating limit in the same enclosure as the modules.
The VFD68 drive has been approved for use in an enclosure. Approval tests were conducted under the conditions in Table 1.
When mounting the VFD68 drive in an enclosure, ensure that the specified space around the drive is maintained, and that the ambient conditions are within the specified limits.
Important: The VFD68 Drive is intended to be mounted in an enclosure that only
allows access by trained and authorized personnel, and that prevents the ingress of
contamination. It is designed for use in an environment classified as pollution degree 2
in accordance with IEC 60664-1. This means that only dry, non-conducting contamination
is acceptable.
| Surrounding Air Temperature1 | -40
to 50°C (-40 to 122°F) as measured 5 cm from the VFD |
|
| Ambient Humidity | 90% RH or less (Non-condensing) | |
| Storage Temperature | -40 to 65°C (-40 to 149°F) | |
| Atmosphere | Indoors (no corrosive and flammable gases, oil mist, dust and dirt.) | |
| Altitude Limit2: Below 1,000 m (3,280 ft) above sea level | ||
| Vibration Limit: 5.9 m/s (19.4 ft/s) or less at 10–55 Hz (directions of x, y, z axes) | ||
| VFD68Bxx Models | Rated Capacity kW (HP) | Maximum Output Current at 50°C (Amperes) | Maximum Output Current at 60°C (Amperes) | Maximum Output Current at 70°C (Amperes) |
|---|---|---|---|---|
| VFD68BBB | 0.1 (1/8) | 0.8 | 0.6 | 0.5 |
| VFD68BCB | 0.2 (1/4) | 1.4 | 1.1 | 0.9 |
| VFD68BDC | 0.4 (1/2) | 2.5 | 2.1 | 1.7 |
| VFD68BFD | 0.75 (1) | 4.2 | 3.5 | 2.9 |
| VFD68BGG | 1.5 (2) | 7.0 | 5.9 | 4.9 |
| VFD68BHG | 2.2 (3) | 10.0 | 8.5 | 7.0 |
| VFD68BJK | 3.7 (5) | 16.5 | 14.0 | 11.5 |
| VFD68BKL | 5.5 (7-1/2) | 23.8 | 20.2 | 16.6 |
| VFD68BLL | 7.5 (10) | 31.8 | 27.0 | 22.2 |
| VFD68BMP | 11 (15) | 45.0 | 38.2 | 31.5 |
| VFD68BNP | 15 (20) | 58.0 | 49.3 | 40.6 |
| VFD68Bxx Models | Rated Capacity kW (HP) | Maximum Output Current at 50°C (Amperes) | Maximum Output Current at 60°C (Amperes) | Maximum Output Current at 70°C (Amperes) |
|---|---|---|---|---|
| VFD68CDF | 0.4 (1/2) | 1.2 | 1.0 | 0.8 |
| VFD68CFF | 0.75 (1) | 2.2 | 1.8 | 1.5 |
| VFD68CGG | 1.5 (2) | 3.6 | 3.0 | 2.5 |
| VFD68CHH | 2.2 (3) | 5.0 | 4.2 | 3.5 |
| VFD68CJJ | 3.7 (5) | 8.0 | 6.8 | 5.6 |
| VFD68CKL | 5.5 (7-1/2) | 12.0 | 10.2 | 8.4 |
| VFD68CLL | 7.5 (10) | 16.0 | 13.6 | 11.2 |
| VFD68CMP | 11 (15) | 23.0 | 19.6 | 16.1 |
| VFD68CNP | 15 (20) | 29.5 | 25.0 | 20.6 |
| VFD68Dxx Models | Rated Capacity kW (HP) | Maximum Output Current at 50°C (Amperes) | Maximum Output Current at 60°C (Amperes) | Maximum Output Current at 70°C (Amperes) |
|---|---|---|---|---|
| VFD68DFM | 0.75 (1) | 1.7 | 1.4 | 1.1 |
| VFD68DGM | 1.5 (2) | 2.7 | 2.3 | 1.8 |
| VFD68DHM | 2.2 (3) | 4.0 | 3.4 | 2.8 |
| VFD68DJN | 3.7 (5) | 6.1 | 5.1 | 4.2 |
| VFD68DKN | 5.5 (7.5) | 9.0 | 7.6 | 6.3 |
| VFD68DLN | 7.5 (10) | 12.0 | 10.2 | 8.4 |
Figure 1. VFD68Bxx, VFD68Cxx, and VFD68Dxx Maximum Current Output Derating above
50°C

1 Surrounding air temperature is a
temperature measured at a measurement position in an enclosure.
Ambient air temperature is a temperature outside an enclosure. The
VFD68 is designed to operate above 50°C by following the maximum
output current derating limits show in Table 2 and Table 3 and Figure 1.
2 Altitude limit given is for
standard operation of the VFD. For operation at higher altitudes,
derate by 3% for each 500 m (1,640.4 ft), up to a maximum of 2,500 m
(8,202 ft) (91% derating).