Output Terminal LF: Alarm Output (Communication Error Warnings) - PENN Controls - VFD68Bxx - VFD68Cxx - VFD68Dxx - Three‐Phase Motor Speed Controller - VFD68 Three‐Phase Variable Frequency Drive

VFD68 Variable Frequency Drives Technical Bulletin

Product
Document revision
C
Revision date
2019-08-09
Part number
24-7664-3051
During a communication error, the alarm signal (LF signal) is output by the open collector output. Assign the used terminal using P.190, P.192, or P.197 (output terminal function selection).
Figure 1. Alarm Output (Communication Error Warnings)

Note: The LF signal can be assigned to the output terminal using P.190, P.192, or P.197. Changing the terminal assignment may affect the other functions. Make the setting after confirming the function of each terminal.