Outline - PENN Controls - VFD68Bxx - VFD68Cxx - VFD68Dxx - Three‐Phase Motor Speed Controller - VFD68 Three‐Phase Variable Frequency Drive

VFD68 Variable Frequency Drives Technical Bulletin

Product
Document type
Technical Bulletin
Document revision
C
Revision date
2019-08-09
Part number
24-7664-3051

The Modbus protocol performs serial communication between the master and subordinate (VFD) using the dedicated message frame. The dedicated message frame has functions that can read and write data. Using these functions, you can:

  • read and write the parameter values from the VFD
  • write the input commend of the VFD
  • check the operating status

The master communicates with the subordinate (VFD) by accessing the assigned holding register address.

Note: There are two different serial transmission modes: ASCII (American Standard Code for Information Interchange) and RTU (Remote Terminal Unit) mode. This product supports only the RTU mode, in which 1-byte (8-bit) data is transmitted as it is. Only the communication protocol is defined by the Modbus protocol - the physical layer is not stipulated.