| Register | Definition | Read/Write | Remarks |
|---|---|---|---|
| 40002 | VFD Reset | Write | Any value can be written. |
| 40003 | Parameter Clear | Write | Set H965A as a written value. |
| 40004 | All Parameters Clear | Write | Set H965A as a written value. |
| 40006 | Parameter Clear1 | Write | Set H965A as a written value. |
| 40007 | All Parameters Clear1 | Write | Set H965A as a written value. |
| 40009 | VFD Status/Control Input Instruction2 | Read/Write | See below.2 |
| 40010 | Operation Mode/VFD Setting3 | Read/Write | See below.3 |
| 40014 | Running Frequency (RAM Value) | Read/Write | According to the P. 37 settings, the frequency and selectable speed are in 1 rotation/minute increments. |
| 40015 | Running Frequency (EEPROM Value) | Write |
| Bit | Definition | |
|---|---|---|
| Control Input Instruction | VFD Status | |
| 0 | Stop command | RUN (VFD operational)4 |
| 1 | forward rotation command | Forward rotation |
| 2 | reverse rotation command | During reverse rotation |
| 3 | RH (high-speed operation command)5 | SU (up-to-frequency) |
| 4 | RM (middle-speed operation command)5 | OL (overload) |
| 5 | RL (low-speed operation command)5 | 0 |
| 6 | 0 | FU (frequency detection) |
| 7 | RT (second function selection) | ABC (fault) 1 |
| 8 | AU (terminal 4 input selection) | 0 |
| 9 | 0 | 0 |
| 10 | MRS (output stop) | 0 |
| 11 | 0 | 0 |
| 12 | 0 | 0 |
| 13 | 0 | 0 |
| 14 | 0 | 0 |
| 15 | 0 | Fault occurrence |
| Register | Description | Unit |
|---|---|---|
| 40201 | Output Frequency/Speed | 0.01 Hz6 |
| 40202 | Output Current | 0.01 A |
| 40203 | Output Voltage | 0.1 V |
| 40205 | Output Frequency/Speed Setting | 0.01 Hz/1 1 |
| 40208 | Converter Output Voltage | 0.1 V |
| 40209 | Regenerative Brake Duty | 0.1% |
| 40210 | Electronic Thermal Relay Function Load Factor | 0.1% |
| 40211 | Output Current Peak Value | 0.01 A |
| 40212 | Converter Output Voltage Peak Value | 0.1 V |
| 40214 | Output Power | 0.01 kW |
| 40215 | Input Terminal Status7 | – |
| 40216 | Output Terminal Status7 | – |
| 40220 | Cumulative Energization Time | 1 h |
| 40223 | Actual Operation Time | 1 h |
| 40224 | Motor Load Factor | 0.1% |
| 40225 | Cumulative Power | 1 kWh |
| 40252 | PID Setpoint | 0.1% |
| 40253 | PID Measured Value | 0.1% |
| 40254 | PID Deviation | 0.1% |
| 40261 | Motor Thermal Load Factor | 0.1% |
| 40262 | VFD Thermal Load Factor | 0.1% |
| 40263 | Cumulative Power 2 | 0.01 kWh |
| 40264 | PTC Thermistor Resistance | 0.01 k |
| b15 to b7 | b6 | b5 | b4 | b3 | b2 | b1 | b0 | |
|---|---|---|---|---|---|---|---|---|
| Input Terminal Monitor Details | – | RH | RM | RL | – | – | STR | STF |
| Output Terminal Monitor Details | – | – | ABC | – | – | – | – | RUN |
| Parameter | Register | Parameter Name | Read/Write | Remarks |
|---|---|---|---|---|
| P. 0 to P.999 | 41000 to 41999 | See the VFD68Bxx and VFD68Cxx Drive Basic and Advanced Parameters and VFD68Dxx Drive Parameters for the parameter names. | Read/Write | The parameter number +41000 is the register number. |
| C 2 (P.902) | 41902 | Terminal 2 Frequency Setting Bias Frequency | Read/Write | |
| C 3 (P.902) | 42092 | Terminal 2 Frequency Setting Bias (Analog Value) | Read/Write | The analog value (%) set to C 3 (P.902) is read. |
| 43092 | Terminal 2 Frequency Setting Bias (Terminal Analog Value) | Read | The analog value (%) of the voltage (current) applied to terminal 2 is read. | |
| P.125 (P.903) | 41903 | Terminal 2 Frequency Setting Gain Frequency | Read/Write | |
| C 4 (P.903) | 42903 | Terminal 2 Frequency Setting Gain (Analog Value) | Read/Write | The analog value (%) set to C 4 (P.903) is read. |
| 43903 | Terminal 2 Frequency Setting Gain (Terminal Analog Value) | Read | The analog value (%) of the voltage (current) applied to terminal 2 is read. | |
| C 5 (P.904) | 41904 | Terminal 4 Frequency Setting Bias Frequency | Read/Write | |
| C 6 (P.904) | 42904 | Terminal 4 Frequency Setting Bias (Analog Value) | Read/Write | The analog value (%) set to C 6 (P.904) is read. |
| 43904 | Terminal 4 Frequency Setting Bias (Terminal Analog Value) | Read | The analog value (%) of the voltage (current) applied to terminal 4 is read. | |
| P.126 (P.905) | 41905 | Terminal 4 Frequency Setting Gain Frequency | Read/Write | |
| C 7 (P.905) | 42905 | Terminal 4 Frequency Setting Gain (Analog Value) | Read/Write | The analog value (%) set to C 7 (P.905) is read. |
| 43905 | Terminal 4 Frequency Setting Gain (Terminal Analog Value) | Read | The analog value (%) of the voltage (current) applied to terminal 4 is read. |
| Register | Definition | Read/Write | Remarks |
|---|---|---|---|
| 40501 | Fault History 1 | Read/Write | Data is 2-bytes long, so is stored as H00OO. Refer to the lowest 1-byte for the error code. Perform write using the register 40501 batch-clears the faults history. Set any value as data. |
| 40502 | Fault History 2 | Read | |
| 40503 | Fault History 3 | Read | |
| 40504 | Fault History 4 | Read | |
| 40505 | Fault History 5 | Read | |
| 40506 | Fault History 6 | Read | |
| 40507 | Fault History 7 | Read | |
| 40508 | Fault History 8 | Read |
| Data | Definition | Data | Definition | Data | Definition |
|---|---|---|---|---|---|
| H00 | No fault present | H31 | E.THM | HB0 | E.PE |
| H40 | E.FIN | HB1 | E.PUE | ||
| H10 | E.OC1 | H52 | E.ILF | HB2 | E.RET |
| H11 | E.OC2 | H60 | E.OLT | HC0 | E.CPU |
| H12 | E.OC3 | H70 | E.BE | HC4 | E.CDO |
| H20 | E.OV1 | H80 | E.GF | HC5 | E.IOH |
| H21 | E.OV2 | H81 | E.LF | HC7 | E.AIE |
| H22 | E.OV3 | H90 | E.OHT | HC9 | E.SAF |
| H30 | E.THT | H91 | E.PTC | HF5 | E.5 |
1 The communication parameter values are
not cleared.
2 For write, set data as the control input
instruction. For read, data is read as a VFD operating
status.
3 For write, set data as the operation mode
setting. For read, data is read as the operation mode
status.
4 The signal within parenthesis is the
initial setting. Definitions change according to the settings for
P.180 to P182.
5 The signal within the parenthesis is the
initial setting. Definitions change according to the settings for
P.190 and P.192.
6 When P. 37 = 0.01 to 9998, this displays
as an integer number.