Broadcast - PENN Controls - VFD68Bxx - VFD68Cxx - VFD68Dxx - Three‐Phase Motor Speed Controller - VFD68 Three‐Phase Variable Frequency Drive

VFD68 Variable Frequency Drives Technical Bulletin

Product
Document revision
C
Revision date
2019-08-09
Part number
24-7664-3051

By specifying address 0, the master can send a message to all subordinates. All subordinates that received the message from the master execute the requested function. In this communication, the subordinates do not return a response to the master.

Note: The VFD performs the function independently of the VFD station number setting (P.117) during broadcast communication.