The VFD68 Drives meet the requirements for their respective rating categories (Table 1).
Rating Category | Suitable for use in a circuit capable of delivering not more than |
---|---|
VFD68Bxx Drives (230 VAC Class) | 100 kA rms symmetrical amperes, 264 V maximum |
VFD68Cxx Drives (460 VAC Class) | 100 kA rms symmetrical amperes, 528 V maximum |