Restarting the Motor After It Has Stopped - PENN Controls - VFD68Bxx - VFD68Cxx - Three‐Phase Motor Speed Controller - VFD68 Three‐Phase Variable Frequency Drive

VFD68 Variable Frequency Drives (230 or 460 VAC) Installation Guide

Product
Document type
Installation Guide
Document revision
F
Revision date
2019-08-16
docpartnumberlabel
Part No.
Part number
24-7664-3108

About this task

To restart the motor after a controlled stop, disconnect the supply power from the drive for at least 30 seconds and then reconnect the supply power to the drive.

If it is not easy to disconnect the supply power from the drive, follow these steps:

Procedure

  1. Disconnect the jumper between the SD and STF terminals on the low-voltage terminal blocks.
  2. Press PU/EXT. The PU LED lights.
  3. Press PU/EXT two more times. The EXT LED lights.
  4. Reconnect the jumper between the SD and STF terminals.