Manually Stopping the Motor - PENN Controls - VFD68Bxx - VFD68Cxx - Three‐Phase Motor Speed Controller - VFD68 Three‐Phase Variable Frequency Drive

VFD68 Variable Frequency Drives (230 or 460 VAC) Installation Guide

Product
Document type
Installation Guide
Document revision
F
Revision date
2019-08-16
docpartnumberlabel
Part No.
Part number
24-7664-3108

You can stop the motor while the VFD68 Drive is in any mode (PU, EXT, or NET) by pressing STOP/RESET. When you press STOP/RESET, the drive monitor displays PS (PU Stop Warning) and then performs a controlled shutdown of the motor.