RUN, MON, PRM LEDs - PENN Controls - VFD68Bxx - VFD68Cxx - Three‐Phase Motor Speed Controller - VFD68 Three‐Phase Variable Frequency Drive

VFD68 Variable Frequency Drives (230 or 460 VAC) Installation Guide

Product
Document revision
F
Revision date
2019-08-16
docpartnumberlabel
Part No.
Part number
24-7664-3108

The RUN, MON, and PRM LEDs provide drive status and indicate the type of information being displayed on the operation panel monitor.

RUN LED: The LED state (on steady, flashing, or flickering) provides information regarding the drive and motor run status. See Figure 1 for more information.

MON LED: Indicates that the monitor is displaying the drive run status. Press (SET) to scroll through run frequency, output amperes, and output voltage.

PRM LED: Indicates that the monitor is set to display parameters and parameter values and allows you to view and edit parameter values.

Figure 1. Operation Panel