Correspondences Between Digital and Actual Characters - PENN Controls - VFD68Bxx - VFD68Cxx - Three‐Phase Motor Speed Controller - VFD68 Three‐Phase Variable Frequency Drive

VFD68 Variable Frequency Drives (230 or 460 VAC) Installation Guide

Product
Document type
Installation Guide
Document revision
F
Revision date
2019-08-16
docpartnumberlabel
Part No.
Part number
24-7664-3108

The actual alphanumeric characters correspond to the following digital characters displayed on the operation panel:

Actual Digital
Actual Digital
Actual Digital