Configuring EXT Mode Using Analog Inputs - PENN Controls - VFD68Bxx - VFD68Cxx - Three‐Phase Motor Speed Controller - VFD68 Three‐Phase Variable Frequency Drive

VFD68 Variable Frequency Drives (230 or 460 VAC) Installation Guide

Product
Document revision
F
Revision date
2019-08-16
docpartnumberlabel
Part No.
Part number
24-7664-3108

About this task

Verify that the VFD68 is in PU mode with no jumper between SD and STF (Figure 1).

Procedure

  1. Verify that the jumper above terminal SC (Figure 1) is set to SINK.
  2. Verify that the AI2 mode switch to the left of terminal A (Figure 1) is set to V for applications with 0–5 V or 0–10 V voltage input or set to I for applications with 4–20 mA current input.
  3. Exit the PU (manual operation) mode by pressing PU/EXT until the EXT LED is highlighted, then use a jumper to connect SD to STF.
    Note: The jumper between SD and STF must be connected for the VFD68 Drive to run.

Results

The VFD68 is now commissioned, is in the external operation mode, and is ready to run the motor using the analog inputs.