Select and Change Most Parameters - PENN Controls - VFD68Bxx - VFD68Cxx - Three‐Phase Motor Speed Controller - VFD68 Three‐Phase Variable Frequency Drive

VFD68 Variable Frequency Drives (230 or 460 VAC) Installation Guide

Product
Document revision
F
Revision date
2019-08-16
docpartnumberlabel
Part No.
Part number
24-7664-3108

Procedure

  1. Turn the Setting dial to select a parameter number on the display. Example: P. 32
  2. Press SET to show the parameter value. (The default value for P. 32 is 12.5.)
  3. Turn the Setting to change the parameter value. (Set P. 32 to 9999 if the motor is to run at minimum speed during low pressure events).
  4. Press SET twice to store the new value.
  5. Press SET again to show the next parameter.

    To select and change the value of another parameter, repeat Step 1 through Step 5.

    To adjust the C-Prefix parameters, go to Select and Change C-Prefix Parameters. If finished, go to Exit the Parameter Adjustment Mode.