Exit the Parameter Adjustment Mode - PENN Controls - VFD68Bxx - VFD68Cxx - Three‐Phase Motor Speed Controller - VFD68 Three‐Phase Variable Frequency Drive

VFD68 Variable Frequency Drives (230 or 460 VAC) Installation Guide

Product
Document revision
F
Revision date
2019-08-16
docpartnumberlabel
Part No.
Part number
24-7664-3108

Procedure

  1. Press MODE twice to exit parameter setting mode (PRM mode) and enter manual operation mode (PU mode). The PU LED illuminates.
  2. Press PU/EXT twice to exit PU mode and enter EXT RUN mode for normal operation. The EXT LED illuminates.
  3. Use the jumper wire to connect terminal SD to terminal STF to run the motor using the analog input.